LTE TDD
For Waveform Playback (ARB) capability.
This topic describes the settings of the Downlink > PRS node for an Advanced TDD Downlink carrier.
Number of Consecutive DL Subframes
Turns the positioning reference signal (PRS) on or off.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS[:STATe] ON|OFF|1|0 [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS[:STATe]? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS OFF :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS? |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Sets the power level, in dB for the positioning reference signal.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:POWer <rel_ampl> [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:POWer? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:POWer 0 :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:POWer? |
|
Range |
-60 to 20 dB |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
-60 |
|
Max |
20 |
|
Initial S/W Revision |
A.20.01 |
Sets the antenna mapping for PRS antenna port 6.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:AMAP <string> [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:AMAP? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:AMAP "1" :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:AMAP? |
|
Range |
0 or 1, as comma separated values (CSV), equal to the number of antennas selected. |
|
Dependencies |
Length equals Total Number of Antennas. |
|
Preset |
"1" |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Sets the number of PDCCH symbols.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:NPDCch <integer> [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:NPDCch? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:NPDCch 1 :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:NPDCch? |
|
Range |
|
|
Couplings |
Coupled to PRS Bandwidth. |
|
Preset |
2 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
3 |
|
Initial S/W Revision |
A.20.01 |
Selects the PRS bandwidth.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:BANDwidth F1400K|F3M|F5M|F10M|F15M|F20M [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:BANDwidth? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:BANDwidth F10M :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:BANDwidth? |
|
Choices |
1.4 MHz (6RB) | 3 MHz (15RB) | 5 MHz (25RB) | 10 MHz (50RB) | 15 MHz (75RB) | 20 MHz (100RB) |
|
Couplings |
PRS Bandwidth must be ≤ System Bandwidth. |
|
Preset |
F10M |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Selects the number of consecutive downlink subframes for PRS.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:NSUBf SF1|SF2|SF4|SF6 [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:NSUBf? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:NSUBf SF1 :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:NSUBf? |
|
Choices |
1 subframe | 2 subframes | 4 subframes | 6 subframes |
|
Preset |
SF1 |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Sets the PRS configuration index. Defines both the periodicity and subframe offset per 3GPP TS 36.211 Table 6.10.2-1.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:CONF <integer> [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:CONF? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:CONF 0 :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:CONF? |
|
Range |
0 to 2399 Formula: (10*SFN + Floor(Slot#/2) - Delta_PRS) mod T_PRS = 0.
|
|
Couplings |
Controls Periodicity and Subframe Offset (read-only). |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
0 |
|
Max |
2399 |
|
Initial S/W Revision |
A.20.01 |
Query only
Displays the PRS periodicity in subframes. Value is set by software based on I_PRS.
Enum Values: SF160, SF320, SF640, SF1280
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:PERiod? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:PERiod? |
|
Notes |
Mapping:
|
|
Dependencies |
Set by software from Configuration Index. |
|
Preset |
SF160 |
|
State Saved |
No |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Query only
Displays the PRS subframe offset. Value is set by software based on Configuration Index(I_PRS).
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:SFOFfset? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:SFOFfset? |
|
Range |
0 to 1279 subframes. Formula:
|
|
Dependencies |
Set by software from Configuration Index. |
|
Couplings |
|
|
Preset |
0 |
|
State Saved |
No |
|
Min |
0 |
|
Max |
1280 |
|
Initial S/W Revision |
A.20.01 |
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:MSEQl SL2|SL4|SL8|SL16 [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:MSEQl? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier<:DLINk:PRS:MSEQl SL2 :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:MSEQl? |
|
Choices |
SL2 | SL4 | SL8 | SL16 |
|
Couplings |
Determines the valid length of Muting Sequence. |
|
Preset |
SL2 |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Sets the muting sequence as comma-separated values.
0 = muting
1 = not muting
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:MSEQ <string> [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PRS:MSEQ? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:MSEQ "0" :RADio:LTETdd:WAVeform:ARB:CCARrier:DLINk:PRS:MSEQ? |
|
Notes |
Bit string. Length must match Muting Sequence Length. |
|
Dependencies |
Length defined by Muting Sequence Length. When Muting Sequence Length is 2 then it is "1,1" When Muting Sequence Length is 4 then it is "1,1,1,1" When Muting Sequence Length is 8 then it is "1,1,1,1,1,1,1,1" When Muting Sequence Length is 16 then it is "1,1,1,1,1,1,1,1,1,1,1,1,1,1,1,1"
|
|
Preset |
1,1 |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |